Solutions

FREE OF FAULTS AND ECONOMICAL

At present there is an increase in the quality and quantity of waste water treatment in Europe. The main impulse for the market is provided by politics and financial aid from the European Union, primarily their directives for municipal sewage and the outline water directive. In the field of water treatment, the drive technology is decisive for the availability and efficiency of pumping and fan stations.

Completely fault-free operation is just as essential as high efficiency. For drive units which operate continuously, energy costs are a very important factor. In addition to the operation of aeration systems, it is mainly the pumps which are the significant factors for electricity consumption in sewage treatment plants. Because of this, NORD DRIVESYSTEMS has used especially efficient drive solutions since 1995.

Through the optimum combination of energy-efficient motor technology and almost loss-free gear units and frequency inverters with energy-saving functions, we ensure economy for purchase and operation.

SPIRAC AB
AGIMIX International
Wastewater Equipm.
ONAS